earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: IP-IO , MP-C, MP-V, RP-C
Funktionaliteter: SmartX IP-kontrollenheter
Produktversion: 2023, 2024, 7.0
2025-03-20

Exporting an Asset List

You export an Asset list when you have completed the capture of controller data. 

To export an Asset list
  1. On the  Project List page, click on the name of the project that you want to export.

  2. Click the  Export  icon.

  3. Use the share options available on your device to send the asset list to the target location of your choice. Each report is a csv (comma-separated values) file which can be opened with Excel.

  4. Close the Share dialog.

  • Asset List Creator
  • Capturing a Device with the Asset List Creator