earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WebReports
Functionalities: Reports
Product version: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
12/16/2021

Factory Supplied Reports

arrow1_rotationEnergy Monitoring Reports arrow1_rotationProduction Reports arrow1_rotationWebReports Diagnostics Reports

Factory supplied reports are reports that are distributed by Schneider Electric. You receive a collection of factory supplied reports when you install WebReports.

The reports provide information regarding user and system activity, alarms, trends, and energy consumption. Each report prompts you to enter filtering criteria for the input parameters. When you click Run report, the report filters the output according to your criteria and generates the report output. You can then view the report and, optionally, save the report as a Word, Excel, or PDF document, or print your report. For more information, see Report Output .

Factory supplied reports populate the Reports folder in WorkStation when WebReports is installed.

For each factory supplied report, the format such as the columns, rows, headers, and footers is defined.

You can use factory supplied reports as the basis for creating your own reports. For more information, see Custom Reports .

Factory supplied reports cannot be renamed or deleted using the Rename or Delete commands that are available in the Manage Reports page at the WebReports Web site. Although it is not recommended, you can rename and delete the report objects that are linked to the factory supplied reports in WorkStation. For more information, see Reports in WorkStation and the WebReports Web Site .

Energy Monitoring Reports

Energy monitoring reports are based on the measurement of energy at meters within a site. You need to create a hierarchy of sites and meters before you generate energy monitoring reports. The meter hierarchy provides the source from which energy reports are generated. Energy monitoring reports are contained in the Energy Monitoring folder.

For more information, see Energy Monitoring Reports .

Production Reports

Production reports are intended to provide ready made reporting on a number of different aspects of the system. Production reports are contained in the Production folder.

For more information, see Production Reports .

WebReports Diagnostics Reports

WebReports Diagnostic reports are intended for diagnostic purposes. They provide you with information about the way the system is set up, and help you troubleshoot the WebReports configuration. WebReports Diagnostic reports are contained within the WebReports Diagnostics folder.

For more information, see WebReports Diagnostic Reports .

  • Energy Monitoring Reports
  • Production Reports
  • WebReports Diagnostic Reports
  • Report Output
  • Custom Reports
  • Reports in WorkStation and the WebReports Web Site