The License Server can be managed through a web-based administration tool called FLEXnet License Administrator. You use the Administration part of the tool to view system information and administer License Server user accounts, alerts, and other configuration.
The FLEXnet License Administrator web page is hosted by the License Server. You use a web browser to connect to the web page via HTTP or HTTPS. The default protocol is HTTP through port 8888, that is on the License Server host itself: http://localhost:8888. The default user name is "admin" and the default password is "admin".
The Flexnet License Administrator has two main parts: Dashboard and Administration. Use the Dashboard to view the status and information of the licenses that are activated on the License Server. Alerts, such as status and expiring licenses, are reported in the Alert pane.
action_zoom_plus_stroke
Figure:
FLEXnet License Administrator, Dashboard part.
Use the Administrator part to view the System information and administer Flexnet License Administrator user accounts, alerts, License Server configuration, or vendor daemon configuration.
action_zoom_plus_stroke
Figure:
FLEXnet License Administrator, Administration part.
For more information about FLEXnet License Administrator, click the FLEXnet License Administrator Help button
action_zoom_plus_stroke
.
License Server Port Number
With a default installation, the License Server port range is set to 27000-27009. A valid number is any unused port between 0 and 64000.
action_zoom_plus_stroke
Figure:
FLEXnet License Administrator, License Server Configuration
If the License Server uses other ports than the default port range 27000-27009, the port has to be added in front of the @ in the License Server address on the WorkStation, Enterprise Server, or Client tools.
For more information, click FLEXnet License Administrator
Help
button
action_zoom_plus_stroke
.
FLEXnet License Administrator Port Number
The port number to the FLEXnet License Administrator is configured in the file “server.xml” located on the License Server. The path to the file is: C:\Program Files\Schneider Electric EcoStruxure\Building Operation x.y\License Server\conf, where x.y is the version number. The “port” attribute is found within the “webServer” tag.
action_zoom_plus_stroke
Figure:
The port attribute is embedded in the “webServer” tag.