earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: ​License Administrator, ​License Server
Функции: Управление лицензиями
Версия продукта: 2024
03.12.2024

Accessing License Server Using the Interface

You access License Server using the interface to configure the settings, for example, change the port number to the License Server.

To access License Server Using the Interface
  1. On a computer that has access to the the same network as the License Server, to configure is located, open a web browser.

  2. In the address field, type the License Server IP or network. End the address with a colon and then the port number.

    Примечание
    • License Server has the HTTP protocol through port 8888 set as the default. For example: http://162.192.10.1:8888

      The default user name is: admin .

      The default password is: admin .

  3. If you log on for the first time you might be prompted to change password.

For more information, click the Help button

 
action_zoom_plus_stroke
in the License Server interface.