earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Användargränssnitt

Användargränssnitt


Produkter: AS-B, Edge Server, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funktionaliteter: Grundläggande funktionalitet
Produktversion: 2024, 7.0
2024-12-03

Actions Menu – Advanced Submenu

Use the Advanced submenu to peform advanced operations, such as repairing communications or references.

 
action_zoom_plus_stroke The Actions menu - Advanced submenu
Figur: The Actions menu - Advanced submenu

Command

Description

Add attachment

Click to add an alarm attachment to one or several alarms.

Clear Content Type

Click to clear a content type applied on a folder or container object. Mer information finns i Content Types .

Copy attachments from

Click to copy alarm attachments from one alarm to one or several other alarms.

Detect Subnet/Node conflicts

Click to detect address conflicts in the network. The command finds and presents the neuron IDs of any online devices that share the same subnet/node address.

Repair references

Click to repair references when you have moved, renamed, or deleted an object that refers to another object that is offline. Mer information finns i Copy, Paste, Duplicate, Move, Rename, and Delete .

Repair server communication

Click to repair server communication after an EcoStruxure BMS server has been offline. Mer information finns i Repairing EcoStruxure BMS Server Communication .

Rebind

Click to rebind a LonWorks network and clear and recreate all LonWorks bindings.

Remove all attachments

Click to remove all alarm attachments from one or several alarms.

Select Content Type

Click to select a content type that you want to apply to a folder or container object. Mer information finns i Content Types .

Copy properties from…

Click to choose the object that you want to copy properties from.

Change Control

Click to open the Change Control submenu. Mer information finns i Actions Menu – Change Control Submenu .

  • Copy, Paste, Duplicate, Move, Rename, and Delete
  • Actions Menu
  • Repairing EcoStruxure BMS Server Communication
  • EcoStruxure BMS Server Status
  • Adding an Attachment to Multiple Alarms
  • Copying Attachments to Multiple Alarms
  • Removing Attachments from Multiple Alarms
  • Mass Copying Selected Properties
  • Content Types
  • Select Content Type Dialog Box
  • Actions Menu – Change Control Submenu
  • Change Control