earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Explicación de procesos

Explicación de procesos


Productos License Administrator, License Server
Funcionalidades: Gestión de licencias
Versión del producto: 2.0, 2.1, 3.0, 3.1
18/05/2018

Activating a Local License

You activate a local license on a WorkStation, client tool, or Enterprise Server computer to have as a substitute until you have set up an EcoStruxure BMS with available network licenses.

Mostrar más
action_close

Local license are used for demonstration purposes or when building a site.

A local license is installed on the client or on License Server from a license file with the extension .asr. The local license is bound to the computer and cannot be shared. The license file used to activate local licenses can only be used once per computer and is typically time-limited.

 
action_zoom_plus_stroke A local license is activated on the computer that will use it and cannot be shared with other computers.
Figura: A local license is activated on the computer that will use it and cannot be shared with other computers.

For more information on how to order additional licenses, please contact your Schneider Electric vendor.

Aviso

After removing a local license, you must restart the computer or server before a similar network license can be checked out.

Aviso
  • Plan the license management carefully and purchase licenses early to avoid unexpected operational stops caused by expired time limit.

  • For more information on how to order local licenses for client tools, please contact your EcoStruxure BMS vendor.

Mostrar más
action_close

EcoStruxure BMS uses two types of licenses: the network license and the local license. Network licenses are the most common type of license in an EcoStruxure BMS. With network licenses, only the number of licenses that are used at the same time are required. The local license is often time limited and used to test and run a system that is under construction, or for demonstration purpose.

The EcoStruxure Building Operation license policy consists of two major types of licenses:

  • Licenses managed by License Administrator

  • Licenses managed by Device Administrator

Licenses Managed by License Administrator

The License Administrator manage the licenses for the following products:

  • Enterprise Central

  • Enterprise Server

  • Clients, WorkStation and WebStations

  • Tools, Graphic Editor, Script Editor, and Function Block Editor

License Administrator runs on Windows.

Tabla: Licenses Managed by License Administrator

Product license

Feature string 1

Description

Client Station

client.station

Use this license to start and run WorkStation and WebStation.

Client tools

client.graphiceditor

client.script

client.functionblock.view

This license product group consists of several products, each required to run the corresponding client tool.

Licensing of WorkPlace Tech is included with the Script Editor license.

Enterprise Central

server.enterprise.central

Use this license to start and run an Enterprise Central.

Enterprise Server

server.enterprise.base

Use this license to start and run an Enterprise Server.

Enterprise Server under Enterprise Central

server.ec.es

Use this license to attach Enterprise Servers to an Enterprise Central.

Field bus devices under Enterprise Server

server.device.es

Use this license to attach Field bus devices to an Enterprise Server.

SmartX server under Enterprise Server

server.es.as

Use this license to attach SmartX server to an Enterprise Server.

SmartDriver

smartdriver.license

Use this license to allow SmartDrivers.

SNMP Notifications

server.alarms.snmp

Use this license to allow SNMP notifications.

Personal Dashboards

client.dashboard

Use this license to allow Personal Dashboards.

Change Control

server.esignature

Use this license to allow Change Control.

Webservices, EWS Cons

server.ws.ews.consume

Use this license to start and run Web Services, EWS Consume.

Webservices, EWS Cons, SRV

server.ws.ews.server

Use this license to start and run Web Services, EWS Consume.

Webservices, EWS Cons, SRV

server.ws.ews.history

Use this license to start and run Web Services, EWS Consume.

Webservices, Generic Cons

server.ws.generic.consume

Use this license to start and run Web Services.

Cloud Connectivity

server.cloud.demo

Use this license to allows the server to connect to the cloud using Cloud Connectivity.

Cloud Connectivity

server.cloud.customer

Use this license to allow the server to connect to the cloud using Cloud Connectivity.

1 Feature string is visible in License Administrator, in the Diagnostic tab.

Licenses Managed by Device Administrator

The licenses for SmartX server are managed by Device Administrator. This is true both for standalone SmartX servers as well as for SmartX servers attached to an Enterprise Server.

Tabla: Licenses Managed by Device Administrator

Product license

Feature string

Description

SmartDriver

smartdriver.license

Use this license to allow SmartDrivers.

SNMP Notifications

server.alarms.snmp

Use this license to allow SNMP notifications.

Personal Dashboard

client.dashboard

Use this license to allow Personal Dashboards.

Cloud Connectivity

server.cloud.customer

Use this license to allow the server to connect to the cloud using Cloud Connectivity.

License files used to activate time-limited local licenses can be distributed under certain circumstances.

Para obtener más información, consulte Local Licenses .

For more information on how to order licenses, please contact your EcoStruxure BMS vendor.

End User License Agreement

When installing the EcoStruxure Building Operation software, make sure that you agree with the Schneider Electric terms and conditions. For operators or other positions that do not install the software, please refer to the “End User License Agreement (EULA)” document distributed by Schneider Electric.

Local Licenses

Local license are used for demonstration purposes or when building a site.

Para obtener más información, consulte Local Licenses .

Network Licenses

Network licenses are distributed from the License Server. The License Server shares a predetermined number of simultaneous instances that are available network-wide. To start licensed clients and EcoStruxure BMS servers using network licenses, the ​required number of licenses have to be ​available on the License Server.

Para obtener más información, consulte Network Licenses .

Time-Limited Licenses

A time-limited license is a license that gives license rights for a predetermined period of time, usually 30 days. When the time period is over, the license expires. These licenses are distributed as local licenses.

Aviso

To avoid critical stops, purchase permanent licenses before the time limited-licenses expire.

License Selection Process

When a licensed WorkStation, WebStation, client tool, Enterprise Server or Enterprise Central starts, it first checks if a local license is available. If a local license is not available or has expired, the WorkStation, Enterprise Server, or Enterprise Central checks out a network license from a License Server. If no license is available, the WorkStation, client tool, Enterprise Server, or Enterprise Central does not start.

Para obtener más información, consulte License Selection Process .

Inherited Licenses

Inherited licenses are used in multi-server systems.

Para obtener más información, consulte Inherited Licenses .

To activate a local license
  1. In License Administrator, click the Licenses tab.

  2. On the Licenses toolbar, click the Add license from file button

     
    action_zoom_plus_stroke
    .

  3. Select the license file and then click Open .

  4. Click Close .

  5. Click Restart now to restart the License Server and activate the local license.

The local license is now activated and the WorkStation, client tool, or Enterprise Server can start.

  • Removing a Local License or Returning a Network License
  • Licenses
  • Licenses View
  • Licenses View Toolbar
  • Diagnostics View