earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : License Administrator, License Server
Fonctionnalités : Gestion des licences
Version produit : 3.2, 3.3
15/07/2020

Activating an EcoStruxure Building Operation Demo License

You activate EcoStruxure Building Operation demo licenses for demonstration, training, or when building a site.

Afficher plus
action_close

Demo licenses are used for demonstration purposes, training, or when building a site.

EcoStruxure Building Operation Software Demo Licenses Management

Demo licenses for EcoStruxure Building Operation software are local, bound to the computer, and cannot be shared.

Pour plus d'informations, voir EcoStruxure Building Operation Demo License Management .

Automation Server Demo License

There are no demo licenses for stand alone automation servers.

To be able to use features on a SpaceLogic device for demonstration purposes, training, or when building a site, you must use the EcoStruxure Building Operation Software Demo Licenses. The automation server must be attached to an Enterprise Server that uses the inherited licenses.

Pour plus d'informations, voir Inherited Licenses .

Déclaration
  • Plan the license management carefully and purchase licenses early to avoid unexpected operational stops caused by the demo licenses expired time limit.

  • For more information on how to order local licenses for client tools, please contact your EcoStruxure BMS vendor.

Afficher plus
action_close

It is recommended that License Administrator and License Server run on the same computer as Enterprise Server or Enterprise Central that use the licenses.

Schneider Electric recommends that you install the license server framework before installing other EcoStruxure Building Operation software applications and automation servers. License Server installation is included in the License Administrator license package. During the installation of WorkStation, Enterprise Server, or Enterprise Central, the installation software asks for the address to License Server.

In this example, the License Server and Enterprise Server are located on the same computer. Several WorkStations check out licenses from the License Server through the local area network. Licenses are activated on the License Server by the License Activation Server that is controlled by Schneider Electric.

 
action_zoom_plus_stroke WorkStation system with License Server and Enterprise Server on same computer and WorkStation in separate computers, one computer with client tool.
Figure : WorkStation system with License Server and Enterprise Server on same computer and WorkStation in separate computers, one computer with client tool.

When you activate a license, the license is transferred from the License Activation Server to your License Server. When activating a license, details about the transaction and registration details are stored with the license on the License Server.

License Server Installation and Location

License Identification Overview

Use one separate License Server for every Enterprise Central and Enterprise Server to get an overview of your licenses. If two or more Enterprise Servers or Enterprise Centrals gets their licenses from the same License Server, you cannot identify which Enterprise Server or Enterprise Central got the license.

If you need to repair or move an EcoStruxure Building Operation software license, the request must come from the License Server that was used to activate the license.

If you try to install Enterprise Server or Enterprise Central on a computer without a License Administrator, you get the system alarm "Invalid license server configuration". 

License Server Location

Install the License Server and Enterprise Server or Enterprise Central on the same computer to avoid license problems caused by network problems. Use the address @localhost so the Enterprise Server cannot connect to the License server through the network.

License Server Internet access

Ensure that the License Server has access to the Internet and to the local area network. Internet access is necessary when performing tasks that require communication with the License Activation Server, such as activating or returning licenses on your License Server. Instant access to the local area network ensures that licensed WorkStations, client tools, Enterprise Servers, and Enterprise Centrals can check out and check in licenses.

Déclaration

For security reasons, Internet access can be disconnected when communication with the License Activation Server is not needed.

License Administrator Installation and Location

Install License Administrator on the same computer as the Enterprise Server or Enterprise Central. This makes your system less vulnerable to network failure.

To activate an EcoStruxure Building Operation demo license
  1. In License Administrator, click the Licenses tab.

  2. On the Licenses toolbar, click the Add license from file button

     
    action_zoom_plus_stroke
    .

  3. Select the license file and then click Open .

  4. Click Close .

  5. Click Restart now to restart the License Server and activate the local license.

The demo license is now activated and WorkStation, client tool, Enterprise Server or Enterprise Central can start.

  • Removing an EcoStruxure Building Operation Software Demo License
  • EcoStruxure Building Operation Software Licensing Installation and Location
  • Licenses View
  • Licenses View Toolbar
  • Diagnostics View