earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: ​License Administrator, ​License Server
功能: 许可证管理
产品版本: 1.8, 1.9
2015/5/22

Activating a Local License

You activate a local license on a WorkStation, client tool, or Enterprise Server computer, to have as a substitute until you have set up a Building Operation system with available network licenses.

显示更多
action_close

A local license installs on the client or License Server from a license file with the extension .asr. The local license is bound to the computer and cannot be shared. The license file used to activate local licenses can only be used once per computer and is typically time-limited.

 
action_zoom_plus_stroke A local license is activated on the computer that will use it and cannot be shared with other computers.
图: A local license is activated on the computer that will use it and cannot be shared with other computers.

For more information on how to order additional licenses, please contact your Schneider Electric vendor.

注释:

After removing a local license, you must restart the computer or server before a similar network license can be checked out.

注释:
  • Plan the license management carefully and purchase licenses early to avoid unexpected operational stops caused by expired time limit.

  • For more information on how to order local licenses for client tools, please contact your Building Operation vendor.

显示更多
action_close

Building Operation uses two types of licenses: the network license and the local license. Network licenses are the most common type of license in Building Operation. With network licenses, only the number of licenses that are used at the same time are required. The local license is often time limited and used to test and run a system that is under construction.

The Building Operation license policy consists of the following licenses:

表格: Building Operation Licenses

License

File Name

Description

Client Station

client.station

Use this license to start and run WorkStation.

Client tool licenses

client.graphiceditor

client.script

client.functionblock.view

This license product group consists of several products, each required to run the corresponding client tool.

Licensing of WorkPlace Tech is included with the Script Editor license.

Enterprise Server

server.enterprise.base

Use this license to start and run an Enterprise Server.

License files used to activate time-limited local licenses can be distributed under certain circumstances.

有关更多信息,请参阅 Local Licenses .

For more information on how to order licenses, please contact your Building Operation vendor.

End User License Agreement

When installing Building Operation, make sure that you agree with the Schneider Electric terms and conditions. For operators or other positions that do not install the software, please refer to the “End User License Agreement (EULA)” document distributed by Schneider Electric.

Local Licenses

A local license installs on the client or License Server from a license file with the extension .asr. The local license is bound to the computer and cannot be shared. The license file used to activate local licenses can only be used once per computer and is typically time-limited.

有关更多信息,请参阅 Local Licenses .

Network Licenses

Network licenses are distributed from the License Server. The License Server shares a predetermined number of simultaneous instances that are available network-wide. To start licensed clients and SmartStruxure servers using network licenses, the ​required number of licenses have to be ​available on the License Server.

有关更多信息,请参阅 Network Licenses .

Time-Limited Licenses

A time-limited license is a license that gives license rights for a predetermined period of time, usually 30 days. When the time period is over, the license expires. These licenses are distributed as local licenses.

注释:

To avoid critical stops, purchase permanent licenses before the time limited-licenses expire.

Permanent License

A permanent license does not expire.

注释:

To avoid critical stops, purchase permanent licenses before the time limited-licenses expire.

License Selection Process

When a licensed WorkStation, client tool, or Enterprise Server starts, it first checks if a local license is available. If a local license is not available or has expired, the WorkStation or Enterprise Server checks out a network license from a License Server. If no license is available, the WorkStation, client tool, or Enterprise Server does not start.

有关更多信息,请参阅 License Selection Process .

To activate a local license
  1. In License Administrator, click the Licenses view.

     
    action_zoom_plus_stroke
  2. On the Licenses toolbar, click the Add license from file button

     
    action_zoom_plus_stroke
    .

  3. Select the license file and then click Open .

     
    action_zoom_plus_stroke
  4. Click Close .

     
    action_zoom_plus_stroke
  5. Click Restart now to restart the License Server and activate the local license.

     
    action_zoom_plus_stroke

The local license is now activated and the WorkStation, client tool or Enterprise Server can start.

  • Removing a Local License or Returning a Network License
  • Licenses
  • Diagnostics View