earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: ​License Administrator, ​License Server
Functionalities: License Management
Product version: 1.8, 1.9
5/22/2015

Activating Network Licenses

You activate network licenses, from the License Activation Server, to make network licenses for ​WorkStations, Enterprise Servers and client tools available networkwide.

Note:
  • This procedure requires that an order is placed and the entitlement certificate is received. For more information on how to place an order, contact your Building Operation vendor.

Show More
action_close

Building Operation uses two types of licenses: the network license and the local license. Network licenses are the most common type of license in Building Operation. With network licenses, only the number of licenses that are used at the same time are required. The local license is often time limited and used to test and run a system that is under construction.

The Building Operation license policy consists of the following licenses:

Table: Building Operation Licenses

License

File Name

Description

Client Station

client.station

Use this license to start and run WorkStation.

Client tool licenses

client.graphiceditor

client.script

client.functionblock.view

This license product group consists of several products, each required to run the corresponding client tool.

Licensing of WorkPlace Tech is included with the Script Editor license.

Enterprise Server

server.enterprise.base

Use this license to start and run an Enterprise Server.

License files used to activate time-limited local licenses can be distributed under certain circumstances.

For more information, see Local Licenses .

For more information on how to order licenses, please contact your Building Operation vendor.

End User License Agreement

When installing Building Operation, make sure that you agree with the Schneider Electric terms and conditions. For operators or other positions that do not install the software, please refer to the “End User License Agreement (EULA)” document distributed by Schneider Electric.

Local Licenses

A local license installs on the client or License Server from a license file with the extension .asr. The local license is bound to the computer and cannot be shared. The license file used to activate local licenses can only be used once per computer and is typically time-limited.

For more information, see Local Licenses .

Network Licenses

Network licenses are distributed from the License Server. The License Server shares a predetermined number of simultaneous instances that are available network-wide. To start licensed clients and SmartStruxure servers using network licenses, the ​required number of licenses have to be ​available on the License Server.

For more information, see Network Licenses .

Time-Limited Licenses

A time-limited license is a license that gives license rights for a predetermined period of time, usually 30 days. When the time period is over, the license expires. These licenses are distributed as local licenses.

Note:

To avoid critical stops, purchase permanent licenses before the time limited-licenses expire.

Permanent License

A permanent license does not expire.

Note:

To avoid critical stops, purchase permanent licenses before the time limited-licenses expire.

License Selection Process

When a licensed WorkStation, client tool, or Enterprise Server starts, it first checks if a local license is available. If a local license is not available or has expired, the WorkStation or Enterprise Server checks out a network license from a License Server. If no license is available, the WorkStation, client tool, or Enterprise Server does not start.

For more information, see License Selection Process .

To activate network licenses
  1. In License Administrator, click the Licenses view.

     
    action_zoom_plus_stroke
  2. On the Licenses toolbar, click the Add license from entitlement ID button

     
    action_zoom_plus_stroke
    .

  3. In the Enter license entitlement ID box, type the entitlement ID that contains the licenses to activate.

     
    action_zoom_plus_stroke
    Note:
    • The entitlement ID is printed on the entitlement certificate.

  4. Click OK .

  5. In the Activate column, select the number of license to activate.

     
    action_zoom_plus_stroke
  6. Click Activate .

  7. Click Close .

     
    action_zoom_plus_stroke
  8. Click Restart now to restart the License Server and activate the network license.

     
    action_zoom_plus_stroke

The activated licenses are now available on the License Server.

  • Network License Management
  • Licenses
  • Licenses View Icons
  • Opening the Transaction Error Dialog Box