earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Användargränssnitt

Användargränssnitt


Produkter: WebStation
Funktionaliteter: Lokalisering
Produktversion: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-10-29

Add or Remove Languages Dialog Box

Use the Add or remove languages dialog box to add or remove language that can be selected in WebStation.

 
action_zoom_plus_stroke Add or remove languages dialog box
Figur: Add or remove languages dialog box

Tabell: Add or Remove Languages Dialog Box

Component

Description

Upload new language

Click to add a language to the list. Mer information finns i Language Packages .

Remove

Click to remove the selected language. Mer information finns i Language Packages .

  • Language Packages