Produkty: AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funkcje: Alarmy
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Add Cause Note Dialog Box

Use the Add Cause Note dialog box to add a cause note.

 
action_zoom_plus_stroke Add Cause Note dialog box
Rysunek: Add Cause Note dialog box

Tabela: Add Cause Note Dialog Box

Component

Description

Name

Type the name of the cause note.

Group name

Enter the cause note group the cause note belongs to.

Description

Type a description of the cause note.

  • User Actions
  • Control Panel
  • Cause Notes
  • Alarm Control Panel – Cause Notes View