earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmes
Versão do produto: 3.2, 3.3, 2022
15-10-2020

Add Cause Note Dialog Box

Use the Add Cause Note dialog box to add a cause note.

 
action_zoom_plus_stroke Add Cause Note dialog box
Imagem: Add Cause Note dialog box

Tabela: Add Cause Note Dialog Box

Component

Description

Name

Type the name of the cause note.

Group name

Enter the cause note group the cause note belongs to.

Description

Type a description of the cause note.

  • User Actions
  • Control Panel
  • Cause Notes
  • Alarm Control Panel – Cause Notes View