earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : AS-B, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Fonctionnalités : Calendriers
Version produit : 3.2, 3.3, 2022
15/10/2020

Adding a Calculated Date Calendar Event

You add a calculated date to specify a recurring event, such as Friday of the first week of even months. Calculated dates are also used for events or holidays that do not always fall on the same date each year.

Afficher plus
action_close

The dates specified in a calendar are shown in the date list. You can specify dates in a calendar by three different methods:

  • Date: a specific date

  • Date range: a fixed period with a set start and stop date

  • Calculated date: a fixed period that repeats

Date Calendar Events

A single date within a calendar is an entry that occurs once or every year on the same date.

The following single date entry choices schedule an event on a single date, January 1, 2009:

  • Year - 2009

  • Month - January

  • Day of month - 1

  • Day of week - Any day

The following single date entry choices schedule an event on a single date every year, January 1:

  • Year - Any Year

  • Month - January

  • Day of month - 1

  • Day of week - Any day

The following choices produce an error message:

  • A day, month, and year combination that does not coincide

    An example is Friday, March 5, 2009. This date actually falls on a Thursday.

  • Any years past 2105

  • An explicit day that is out of range

    An example is September 31 or February 29 in a non-leap year.​​

Date Range Calendar Events

You can include a date range in the date list. A date range is a series of days to include in a calendar. An example of a date range is January 1, 2009 to January 31, 2009, which adds the entire month of January to the calendar as an event. You can use this date range for a device, such as a thermostat, to behave differently for the whole month of January.

Calculated Calendar Events

You can include a calculated date on a date list. A calculated date has no set start and stop date. For example, you use a calculated date to schedule the first week of the even months on a Friday.

To add a calculated date calendar event
  1. In WorkStation, in the System Tree pane, select the calendar that you want to add the exception dates to.

  2. Click the Calendar Editor tab.

  3. On the Calendar Editor toolbar, click the Add Calculated button

     
    action_zoom_plus_stroke
    .

  4. In the Edit Calendar Entry dialog box, in the Entry name box, type the name that you want to display on the date list.

  5. In the Month box, select a month for the calculated date.

  6. In the Week of month box, select the week of month for the calculated date.

  7. In the Day of week box, select a weekday for the calculated date.

  8. Click OK .

  9. On the File menu, click Save .

  • Adding a Date Calendar Event
  • Adding a Date Range Calendar Event
  • Creating a Calendar
  • Adding a Calendar Exception Event
  • Edit Calendar Entry Dialog Box – Calculated Date
  • Calendars in WorkStation
  • Calendar Events
  • General Information Properties – Basic Tab
  • References Tab