earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Edge Server, Enterprise Server, AS-P, WorkStation, Virtual Project Servers
Functionalities: Schedules
Product version: 2023
12/17/2022

Adding a Calculated Exception Event

You create a calculated exception to schedule a recurring event that takes precedence over a scheduled weekly event.

To add a calculated exception event
  1. In WorkStation, in the System Tree pane, select the schedule you want to add the calculated exception event to.

  2. Click the Basic tab.

  3. On the Basic toolbar, click the New schedule event button

     
    action_zoom_plus_stroke
    .

  4. In the Schedule Event Properties dialog box, under Event type , click Exception .

  5. Under Exception type , click Calculated .

  6. Select All Day to have the event last all day.

  7. In the Name box, type a name for the exception.

  8. In the Priority box, enter a priority.

  9. In the Month box, select a month.

  10. In the Week of month box, select a week of the month.

  11. In the Day of week box, select a day of the week.

  12. Click OK .

  • Exception Events in WorkStation
  • Schedule Event Properties Dialog Box – Calculated Exception View