earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
功能: 时间表
产品版本: 2024, 7.0
2024/12/3

Adding a Calculated Exception Event

You create a calculated exception to schedule a recurring event that takes precedence over a scheduled weekly event.

To add a calculated exception event
  1. In WorkStation, in the System Tree pane, select the schedule you want to add the calculated exception event to.

  2. Click the Basic tab.

  3. On the Basic toolbar, click the New schedule event button

     
    action_zoom_plus_stroke
    .

  4. In the Schedule Event Properties dialog box, under Event type , click Exception .

  5. Under Exception type , click Calculated .

  6. Select All Day to have the event last all day.

  7. In the Name box, type a name for the exception.

  8. In the Priority box, enter a priority.

  9. In the Month box, select a month.

  10. In the Week of month box, select a week of the month.

  11. In the Day of week box, select a day of the week.

  12. Click OK .

  • Exception Events in WorkStation
  • Schedule Event Properties Dialog Box – Calculated Exception View