Productos AS-L, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmas
Versión del producto: 2.0, 2.1, 3.0, 3.1
04/09/2018

Adding a Cause Note to an Alarm

You add a cause note to an alarm to report the cause of the alarm.

Mostrar más
action_close

A cause note specifies the problem that caused the alarm. Cause notes are grouped by category, with possible alarm causes listed in each group. When an alarm is triggered, you can easily report the causes that triggered the alarm by selecting the predefined choices.

 
action_zoom_plus_stroke Cause Notes dialog box
Figura: Cause Notes dialog box

Reporting the cause of the alarm is either voluntary or mandatory. You can configure the alarm so the user is required to report the causes when certain events occur, such as when an alarm is disabled.

​Cause notes can be of great use the next time the same alarm is triggered or when extracting alarm statistics.

To add a cause note to an alarm
  1. In WorkStation, in the System Tree pane, select the alarm object to which you want to add a cause note.

  2. In the User Action tab, in the Cause note group box, enter the cause note you want to add to the alarm.

  3. Click the Save button

     
    action_zoom_plus_stroke
    .

To add a cause note to an alarm, you must have created one in advance and defined its content.

  • Creating a Cause Note
  • Create Alarm Wizard – User Action Page
  • Cause Notes