earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: WorkStation
Funktionaliteter: Larm
Produktversion: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-05-18

Adding a Comment to an Alarm

You add a comment to an alarm to help others understand the problem that caused the alarm or how the alarm was solved.

Visa mer
action_close

You can add a comment to an alarm that can be helpful the next time the same alarm is triggered.

Other people can read your comment in WorkStation or WebStation. You can add a comment to an alarm that is assigned to yourself or to someone else.

Your comment is marked with your user name and the time you made the comment.

In some cases, adding a comment to an alarm is optional. In other cases, you are required to add a comment when you acknowledge the alarm.

You add a comment using WorkStation or WebStation. You can view a comment added to an alarm in WorkStation and WebStation.

To add a comment to an alarm
  1. In WorkStation, in the Alarms pane, right-click the alarm and then click Add comment .

  2. In the Add Comment dialog box, type the comment.

  3. Click OK .

  • Alarm Comments
  • Viewing an Alarm Comment
  • Alarms Pane and Alarm View
  • Add Comment Dialog Box
  • Alarms Pane Context Menu
  • Alarms Pane and Alarm View Toolbar