Produits : WebStation
Fonctionnalités : Calendriers
Version produit : 2024, 7.0
03/12/2024

Adding a Date to a Calendar

You add a date to a calendar to specify an exception date for a specific day.

Afficher plus
action_close

You specify a single date in a calendar. A date is an entry that occurs once in the calendar.

  • Date: a specific date

A single date within a calendar is an entry that occurs once.

To add a date to a calendar
  1. In WebStation, in the System Tree pane, select the calendar you want to add the exception to.

  2. Click on the date where you want to create the event.

  • Calendar Events
  • Calendars in WebStation
  • Schedule Workspace Toolbar
  • Exception Events in WebStation
  • Calendar Workspace
  • Removing a Calendar Event
  • Adding a Calendar Exception Event