Productos AS-B, Edge Server, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funcionalidades: Programaciones
Versión del producto: 3.2, 3.3, 2022, 2023
21/05/2024

Cómo añadir un evento de excepción de calendario

Puede añadir un evento de excepción de una fecha para que la excepción se aplique a un día específico de la programación, por ejemplo, el 10 de diciembre de 2013.

Mostrar más
action_close

An exception event occurs instead of the scheduled weekly events for a single date, date range, calculated date, or calendar reference.

For example, you create an exception event in March for an intense aerobics class in the gym to open an air vent to 100 % from 06:30 to 17:00 every Wednesday in March. This exception event takes precedence over the regularly scheduled weekly Wednesday events.

When scheduling exception events, you can use four exception types to provide flexibility and control in your schedule.

Date Exception Events

A single date exception event can occur on a single day, or you can use the options for the event to occur on more than one day. The options such as Any year and Any day provide flexibility. To schedule a single date event to take place every year on October 31, you select the following single date options:

  • Year: Any year

  • Month: October

  • Day of month: 31

  • Day of week: Any day

Date Range Exception Events

A date range exception event is an event that lasts over a period of time. In addition to a specific day of month, you can select Odd, Even , or Any month , and Any day or Last day , to provide the flexibility to a date range. For example, to schedule an exception event to occur annually from the last day of March to the last day of April, select the following options for the start and end dates:

Start Date
  • Start year: Any year

  • Start month: March

  • Day of month: Last day

  • Day of week: Any day

End Date
  • Year: Any year

  • Month: April

  • Day of month: Last day

  • Day of week: Any day

Calculated Exception Events

A calculated date is an exception event that recurs. Other than a specific month and week, you can select Any month and Any week or Last week , to provide flexibility to a calculated date. For example, to schedule the Monday of the first week of every month for an exception event, select the following options:

  • Month: Any month

  • Week of month: First week

  • Day of week: Monday

Calendar Exception Events

A calendar reference allows you to apply an exception event for all dates specified in the calendar. For example, to schedule exception events for all holidays on a calendar, you select the calendar you want to reference and the schedule will follow the holidays created in the calendar.

Para añadir un evento de excepción de intervalo de fecha
  1. En WorkStation, en el panel Árbol del sistema , seleccione la programación a la que desea añadir el evento de excepción de única fecha.

  2. Haga clic en la pestaña Básico .

  3. En la barra de herramientas Editor de programación básica , haga clic en el botón Nuevo evento de calendario

     
    action_zoom_plus_stroke
    .

  4. Haga clic en Excepción .

  5. En el cuadro de diálogo Propiedades de eventos de programación , haga clic en el cuadro Tipo de excepción , haga clic en Fecha única .

  6. Seleccione Todo el día si el evento de excepción debe estar activado o desactivado todo el día.

  7. En la columna Hora de inicio , escriba una hora de inicio del evento de excepción.

  8. En la columna Hora de fin , escriba una hora de fin para el evento de excepción.

  9. En la columna Valor , seleccione un valor para el evento de excepción.

  10. En el cuadro Nombre escriba un nombre para el evento de excepción.

  11. En el cuadro Prioridad , seleccione una prioridad para el evento de excepción, para que se omitan eventos en conflicto con prioridades inferiores.

  12. En el cuadro Año , seleccione el año de la fecha simple.

  13. En el cuadro Mes , seleccione el mes de la fecha simple.

  14. En Día del mes , seleccione un día del mes para la fecha simple.

  15. En Día de la semana x, seleccione el día de la semana para la fecha simple.

  16. Haga clic en Aceptar .

  17. En el menú Archivo , haga clic en Guardar .

  • Schedule Events
  • Exception Events in WorkStation
  • Schedule Event Properties Dialog Box – Single Date Exception View