earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
功能: 时间表
产品版本: 2024, 7.0
2024/12/3

Adding a Date Range Exception Event

You create a date range exception to schedule a date range event that takes precedence over a scheduled weekly event.

To add a date range exception event
  1. In WorkStation, in the System Tree pane, select the schedule you want to add the date range exception event to.

  2. Click the Basic view.

  3. On the Basic toolbar, click the New schedule event button

     
    action_zoom_plus_stroke
    .

  4. In the Schedules Event Properties dialog box, under Event type , click Exception .

  5. Under Exception type , click Date range .

  6. Select All Day to have the event last all day.

  7. In the Value box, enter a value.

  8. In the Name box, type a name for the exception.

  9. In the Priority box, select a priority.

  10. In the Year box, select a year for the start date and the end date.

  11. In the Month box, select a month for the start date and end date.

  12. In the Day of month box, select a day of the month for the start date and end date.

  13. In the Day of week box, select a day of the week for the start date and end date.

  14. Click OK .

  • Exception Events in WorkStation
  • Schedule Event Properties Dialog Box – Date Range Exception View