earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 2.0, 2.1, 3.0, 3.1
5/18/2018

Creating a Hyperlink

You create a hyperlink in WorkStation to get easy access to important information on the Internet.

Show More
action_close

The EcoStruxure Building Operation software supports hyperlinks. Hyperlinks can be added and displayed in WorkStation. Hyperlinks can also be added in, for example, a graphic that is displayed in WorkStation. In WorkStation, you can navigate on the web page in same way as in a web browser. 

The EcoStruxure Building Operation software uses Microsoft Internet Explorer to present web pages. Plug-ins, for example Flash and Java, have to be installed to be able to correctly display pages that use these plug-ins.

 
action_zoom_plus_stroke The EcoStruxure Building Operation software supports hyperlinks
Figure: The EcoStruxure Building Operation software supports hyperlinks

To create a hyperlink
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server or folder where you want to create the hyperlink.

  2. On the File menu, point to New and then click Hyperlink .

  3. In the Create Object dialog box, in the Name box, type a name for the hyperlink.

  4. In the Description box, type a description for the hyperlink.

  5. Click Next .

  6. In the Assign the URL page, in the URL box, type the URL for the hyperlink.

    Important:

    You have to include http:// or https:// in the URL.

  7. Click Create .

  • Hyperlinks
  • Create Object Wizard – Naming the Object Page