earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Explicación de procesos

Explicación de procesos


Productos AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Tendencias
Versión del producto: 1.9
14/12/2016

Adding a Trend Log Record to a Manual Trend Log

You have to manually add records to a manual trend log.

Mostrar más
action_close

​The manual trend log records data that you manually enter. The manual trend log does not log a variable. Use this type of trend log when values from offline devices have to be manually registered to the trend log. For example, if you want to create a trend log that monitors an electricity meter that cannot be connected to Building Operation.

 
action_zoom_plus_stroke Manual trend log schematic.
Figura: Manual trend log schematic.

To add a trend log record to a manual trend log
  1. In WorkStation, in the System Tree pane, select the folder or SmartStruxure server where the trend log is located.

  2. Select the manual trend log you want add a value to.

  3. On the Actions menu, point to Modification, and then click Add log record .

  4. In the Time stamp box, enter the date and time of the new value.

     
    action_zoom_plus_stroke
  5. In the Value box, enter the value.

  6. In the Comment box, type a comment.

  7. Click Add record .

  8. Click Close .

The record is now added to the trend log.

  • Manual Trend Logs
  • Add Trend Log Record Dialog Box
  • Trend Log Lists
  • Cómo editar o comentar una entrada de registro de tendencias
  • Cómo añadir manualmente un registro de tendencias a una lista de registro de tendencias
  • Cómo añadir manualmente un registro de tendencias a una lista de registro de tendencias