earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
功能: 趋势
产品版本: 1.8
2016/10/14

Adding a Trend Log Record to a Manual Trend Log

You have to manually add records to a manual trend log.

显示更多
action_close

​The manual trend log records data that you manually enter. The manual trend log does not log a variable. Use this type of trend log when values from offline devices have to be manually registered to the trend log. For example, if you want to create a trend log that monitors an electricity meter that cannot be connected to Building Operation.

 
action_zoom_plus_stroke Manual trend log schematic.
图: Manual trend log schematic.

注释:
  • The Add trend log record dialog box is only applicable to manual trend logs.

To add a trend log record to a manual trend log
  1. In WorkStation, in the System Tree pane, select the folder or SmartStruxure server where the trend log is located.

  2. Select the manual trend log you want add a value to.

  3. On the Actions menu, point to Modification, and then click Add log record .

  4. In the Time stamp box, type the time of the new value.

     
    action_zoom_plus_stroke
  5. In the Data type box, select Number if the value is an integer or decimal.

  6. In the Value box, type the value.

  7. In the Comment box, type a comment.

  8. Click Add record .

  9. Click Close .

The record is now added to the trend log.

  • Manual Trend Logs
  • Add Trend Log Record Dialog Box
  • Trend Log Lists
  • Editing or Commenting a Trend Log Record