earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Modalità

Modalità


Prodotti: AS-B, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funzionalità: Programmi orari
Versione del prodotto: 3.2, 3.3, 2022
15/10/2020

Adding a Weekly Event

You add weekly events to a schedule to determine when the event is to regularly occur. Weekly events always occur regularly unless overridden by an exception event.

Mostra di più
action_close

A weekly event occurs every week for an extended period of time on a regular basis. You can schedule more than one weekly event for each day of the week.

 
action_zoom_plus_stroke Weekly events in an EcpStruxure Building Operation schedule
Figura: Weekly events in an EcpStruxure Building Operation schedule

If there are any non-routine events, such as holidays, you can use exception events to override the schedule. Per maggior informazioni, consulta Exception Events in WorkStation .

To add a weekly event
  1. In WorkStation, in the System Tree pane, select the schedule you want to add the weekly event to.

  2. Click the Basic tab.

  3. On the Basic Schedule Editor toolbar, click the View weekly schedule events button

     
    action_zoom_plus_stroke
    .

  4. In the grid, click the start time. Drag the cursor vertically to select the end time and then horizontally to select all days for which the event should be valid.

  5. On the File menu, click Save .

  • Adding a Calendar Exception Event
  • Aggiunta di un evento di eccezione per una data
  • Adding a Date Range Exception Event
  • Adding a Calculated Exception Event
  • Basic View of the Schedule Editor
  • Weekly Events in WorkStation
  • Schedule Events