Productos AS-L, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmas
Versión del producto: 2.0, 2.1, 3.0, 3.1
04/09/2018

Adding an Action Note to an Alarm

You add an action note to an alarm to troubleshoot and report the problem that triggered the alarm.

Mostrar más
action_close

​Action notes are grouped by category, with possible actions that may correct the problem listed in each category. An action note specifies the actions that you used to correct the problem that caused the alarm.

 
action_zoom_plus_stroke Action Notes dialog box
Figura: Action Notes dialog box

Reporting the actions that were taken is either voluntary or mandatory. You can configure the alarm so the user is required to report the actions when certain events occur, such as when an alarm is disabled.

​Action notes can be of great use the next time the same alarm is triggered or when extracting alarm statistics.

To add an action note to an alarm
  1. In WorkStation, in the System Tree pane, select the alarm object to which you want to add an action note.

  2. In the User action view, in the Action note group box, enter the action note you want to add to the alarm.

  3. Click the Save button

     
    action_zoom_plus_stroke
    .

To add a checklist to an alarm you must have created one in advance and defined its content.

  • Creating an Action Note
  • Create Alarm Wizard – User Action Page
  • Action Notes