earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funkcje: Alarmy
Wersja produktu: 3.2, 3.3, 2022
2022-07-13

Adding an Action Note to an Alarm

You add an action note to an alarm to troubleshoot and report the problem that triggered the alarm.

Pokaż więcej
action_close

​Action notes are grouped by category, with possible actions that may correct the problem listed in each category. An action note specifies the actions that you used to correct the problem that caused the alarm.

 
action_zoom_plus_stroke Action Notes dialog box
Rysunek: Action Notes dialog box

Reporting the actions that were taken is either voluntary or mandatory. You can configure the alarm so the user is required to report the actions when certain events occur, such as when an alarm is disabled.

​Action notes can be of great use the next time the same alarm is triggered or when extracting alarm statistics.

To add an action note to an alarm
  1. In WorkStation, in the System Tree pane, select the alarm object to which you want to add an action note.

  2. In the User action view, in the Action note group box, enter the action note you want to add to the alarm.

  3. Click the Save button

     
    action_zoom_plus_stroke
    .

To add an action note to an alarm you must have created one in advance and defined its content.

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Alarm Control Panel – Action Notes View
  • Creating an Action Note
  • Editing an Action Note
  • Configuring Forced User Actions
  • Import and Export of Supporting Objects