earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 用户管理
产品版本: 2.0, 2.1, 3.0, 3.1
2018/9/14

Administration Accounts in EcoStruxure BMS Server Local Domain

arrow1_rotationAdmin Account arrow1_rotationReports Administrator Account

You can manage user accounts on a domain controller by logging on to the local domain of the EcoStruxure BMS server, using the local administrator and local reports administrator accounts.

Admin Account

Each EcoStruxure BMS server has a local administrator account, named admin. This account is preferably used to log on to the EcoStruxure BMS server the first time to create a new domain with an administration account. To manage and administrate the new domain, it is recommended that you log on to the domain with your domain administration account.

The local administrator account cannot be changed or deleted.

Reports Administrator Account

SystemReportsService is the user account for the Reporting Agent service. The account allows the Reporting Agent service to log on to the Enterprise Server. This user account is set up during the installation of the Enterprise Server and WorkStation and does not require any configuration.

The SystemReportsService is disabled in Enterprise Central and needs to be configured. The password also needs to be set before the Report Server is used with Enterprise Central.

有关更多信息,请参阅 WebReports User Accounts .

  • Domain Properties
  • WebReports User Accounts
  • Domains
  • User Account Management Overview