earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmes
Versão do produto: 3.2, 3.3, 2022
15-10-2020

Alarm – Basic Settings View

Use the Basic Settings view to view the alarm name, alarm type, or edit the comment to change the description of the alarm.

 
action_zoom_plus_stroke Basic Settings view
Imagem: Basic Settings view

Tabela: Basic Settings View

Property

Description

Alarm type

Displays the type of the alarm object.

Name

Displays the name of the alarm object.

Description

Type a description that describes the alarm object.

  • Alarms Overview
  • Alarm Types