earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: WebReports
功能: 报告
产品版本: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
2021/12/16

Alarm Amount by Type Report

The Alarm Amount by Type report provides information about the number of triggered alarms and organizes the information by alarm type, such as Change of State Alarm and Out of Range Alarm. You can use the report to track the greatest number of triggered alarms by alarm type.

The following table shows the input parameters for the report.

表格: Alarm Amount by Type Input Parameters

Input Parameters

Description

Start report date/time

Specifies the start date and time of the triggered alarms.

End report date/time

Specifies the end date and time of the triggered alarms.

Date range filter

Specifies the date range of an operation, such as an alarm trigger, the running of a report schedule, or a read by the Reporting Agent.

For example, if you select Last 7 days for an alarm report, the report displays information about all alarms that were triggered during the last 7 days. If you select Last 7 days for the Report schedule report, the report displays information about all Report schedules that were run during the last 7 days. If you select Last 7 days for the Reporting Agent report, the report displays information about all Reporting Agent reads that occurred during the last 7 days.

Select Fixed date if you entered a Start report date/time and an End report date/time .

Group interval

Specifies the time interval, such as daily, weekly, for organizing and displaying the number of alarms by type.

Target

Specifies a comparative value. When the report runs, the actual alarm counts by type are compared to the target value.

  • Factory Supplied Reports
  • Production Reports
  • WebReports Submit Form Page