功能: 警报
产品版本: 1.8
2016/10/13

Alarm Objects in Multiple Servers

In a multi-server system, you create alarm objects on the Enterprise Server. These objects, such as checklists and action notes, are inherited by the SmartStruxure server devices that are connected to that Enterprise Server. The copies on the connected SmartStruxure server devices are read-only, so in order to edit them you must edit their source objects on the Enterprise Server. One advantage with this is that you can display the objects and their content on the SmartStruxure server devices even if the Enterprise Server goes offline.

注释:

When an Enterprise Server is connected to a SmartStruxure server device, all existing checklists, action notes, cause notes, and categories on SmartStruxure server device are removed and replaced with the objects from the Enterprise Server.

  • Alarms Overview
  • Multi-server System