earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2023
2022/12/17

Alarm Control Panel Objects in Multiple Servers

In a multi-server system, you create Alarm Control Panel objects, such as checklists and actions notes, on the Enterprise Server or on the Enterprise Central.

Automation servers that are connected to that Enterprise Server inherit Alarm Control Panel objects automatically. The copies on the connected automation servers are read-only, so in order to edit them you must edit their source objects on the Enterprise Server. One advantage with this is that you can display the objects and their content on the automation servers even if the Enterprise Server goes offline.

An Enterprise Server that is connected to the Enterprise Central will not automatically inherit alarm objects.

重要:

You need to export Alarm Control Panel objects from the child server (Enterprise Server or an automation server) and import them to the parent server (Enterprise Central or Enterprise Server) before you synchronize the Alarm Control Panel. During synchronization, all the Alarm Control Panel objects are erased from the child server. In particular, ensure that you secured the Alarm Control Panel of your automation server before adding it to the Enterprise Server. 有关更多信息,请参阅 Synchronizing Alarm Control Panels .

  • Alarms Overview
  • Multi-server Systems
  • Lead and Shadow Relationship
  • Alarm Control Panel Synchronization
  • Synchronizing Alarm Control Panels