Use the Alarms pane context menu to manage the alarms in the Alarms pane.
Command |
Description |
Acknowledge |
Click to acknowledge the alarm state or reset state. For more information, see Alarm Acknowledgements . |
Enable alarm |
Click to enable the alarm. If the alarm state changed, for example from alarm state to normal state during the time the alarm was disabled, the alarm is given the new state once it is enabled. For more information, see Disable and Enable Alarms . |
Disable alarm |
Click to disable the alarm. The alarm is disabled and cannot be acknowledged or reset until it is enabled. For more information, see Disable and Enable Alarms . |
Recheck |
Click to update the current alarm state. |
Show alarm |
Click to show the alarm. For more information, see Hide and Show Alarms . |
Hide alarm |
Click to hide the alarm from the Alarms pane. The alarm is still logged in the event log. For more information, see Hide and Show Alarms . |
Enable state-change logging |
Click to start logging an event each time the alarm is changing its state. For more information, see Alarm State-Change Logging . |
Disable state-change logging |
Click to stop logging an event every time the alarm is changing its state. For more information, see Alarm State-Change Logging . |
Self-assign |
Click to assign the alarm to yourself. For more information, see Alarm Assignments . |
Assign |
Click to assign the alarm to another user. For more information, see Alarm Assignments . |
Reject |
Click to reject the alarm. For more information, see Alarm Assignments . |
Accept |
Click to accept the alarm. For more information, see Alarm Assignments . |
Release |
Click to release an alarm that is assigned to you. For more information, see Alarm Assignments . |
Add comment |
Click to add a comment to the alarm. For more information, see Alarm Comments . |
Add cause note |
Click to add a cause note to the alarm. For more information, see Cause Notes . |
Add action note |
Click to add an action note to the alarm. For more information, see Action Notes . |
Checklist |
Click to view the checklist of the alarm. For more information, see Checklists . |
Turn off visual and audible alert |
Click to turn off visual and audible alert. |
Attachments |
Click to open the file or document that is attached to the alarm. For more information, see Alarm Attachments . |
Go to alarm object |
Click to open the settings of the alarm in the Work area. |
Go to source object |
Click to open the object that triggered the alarm in the Work area. |
View |
Click to view the history, comments, cause notes, action notes, or checklists of an alarm in the work area. For more information, see Alarms Pane Context Menu - View Submenu . |
Alarm View settings |
Click to open the Alarm View settings submenu where you can make a number of Alarm View settings for the current Alarms pane or Alarm View. For more information, see Alarms Pane Context Menu - Alarm View Settings Submenu . |