Use the Alarms pane context menu to manage the alarms in the Alarms pane.
Command |
Description |
Acknowledge |
Click to acknowledge the alarm state or reset state. Więcej informacji zawiera Alarm Acknowledgements . |
Enable alarm |
Click to enable the alarm. If the alarm state changed, for example from alarm state to normal state during the time the alarm was disabled, the alarm is given the new state once it is enabled. Więcej informacji zawiera Disable and Enable Alarms . |
Disable alarm |
Click to disable the alarm. The alarm is disabled and cannot be acknowledged or reset until it is enabled. Więcej informacji zawiera Disable and Enable Alarms . |
Recheck |
Click to update the current alarm state. |
Show alarm |
Click to show the alarm. Więcej informacji zawiera Hide and Show Alarms . |
Hide alarm |
Click to hide the alarm from the Alarms pane. The alarm is still logged in the event log. Więcej informacji zawiera Hide and Show Alarms . |
Enable state-change logging |
Click to start logging an event each time the alarm is changing its state. Więcej informacji zawiera Alarm State-Change Logging . |
Disable state-change logging |
Click to stop logging an event every time the alarm is changing its state. Więcej informacji zawiera Alarm State-Change Logging . |
Self-assign |
Click to assign the alarm to yourself. Więcej informacji zawiera Alarm Assignments . |
Assign |
Click to assign the alarm to another user. Więcej informacji zawiera Alarm Assignments . |
Reject |
Click to reject the alarm. Więcej informacji zawiera Alarm Assignments . |
Accept |
Click to accept the alarm. Więcej informacji zawiera Alarm Assignments . |
Release |
Click to release an alarm that is assigned to you. Więcej informacji zawiera Alarm Assignments . |
Add comment |
Click to add a comment to the alarm. Więcej informacji zawiera Alarm Comments . |
Add cause note |
Click to add a cause note to the alarm. Więcej informacji zawiera Cause Notes . |
Add action note |
Click to add an action note to the alarm. Więcej informacji zawiera Action Notes . |
Checklist |
Click to view the checklist of the alarm. Więcej informacji zawiera Checklists . |
Turn off visual and audible alert |
Click to turn off visual and audible alert. |
Attachments |
Click to open the file or document that is attached to the alarm. Więcej informacji zawiera Alarm Attachments . |
Go to alarm object |
Click to open the settings of the alarm in the Work area. |
Go to source object |
Click to open the object that triggered the alarm in the Work area. |
View |
Click to view the history, comments, cause notes, action notes, or checklists of an alarm in the work area. Więcej informacji zawiera Alarms Pane Context Menu - View Submenu . |
Alarm View settings |
Click to open the Alarm View settings submenu where you can make a number of Alarm View settings for the current Alarms pane or Alarm View. Więcej informacji zawiera Alarms Pane Context Menu - Alarm View Settings Submenu . |