earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 2024, 7.0
12/3/2024

Alarm Trigger Properties – Range Tab

Use the Range tab to configure the range that triggers the alarm.

 
action_zoom_plus_stroke Range tab
Figure: Range tab

Table: Range Tab

Component

Description

First value

Enter the lowest integer value of the range that triggers the alarm.

Last value

Enter the highest integer value of the range that triggers the alarm.

  • Alarm Types
  • Multistate Alarm Properties – Basic Tab