earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Användargränssnitt

Användargränssnitt


Produkter: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funktionaliteter: Larm
Produktversion: 3.2, 3.3, 2022
2020-10-15

Alarm Trigger Properties – Range Tab

Use the Range tab to configure the range that triggers the alarm.

 
action_zoom_plus_stroke Range tab
Figur: Range tab

Tabell: Range Tab

Component

Description

First value

Enter the lowest integer value of the range that triggers the alarm.

Last value

Enter the highest integer value of the range that triggers the alarm.

  • Alarm Types
  • Multistate Alarm Properties – Basic Tab