Funkcje: Podstawowa funkcjonalność
Wersja produktu: 3.2, 3.3, 2022
2021-04-30

Alarm View Properties

Use the Alarm View properties to configure and view the general and object references properties. Więcej informacji zawiera General Information Properties – Basic Tab .

 
action_zoom_plus_stroke Alarm properties
Rysunek: Alarm properties

Property

Description

Display on alarm

Select True to to automatically open and display the attachment when the alarm is going from Normal to Alarm state.

Show milliseconds

Select True to display the alarm timestamp in milliseconds.

  • General Information Properties – Basic Tab
  • Alarms Overview