earth_america
user_standard 登录
action_search_stroke
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2024, 7.0
2024/12/3

Alarm View Properties

Use the Alarm View properties to configure and view the general and object references properties. 有关更多信息,请参阅 General Information Properties – Basic Tab .

 
action_zoom_plus_stroke Alarm properties
图: Alarm properties

Property

Description

Property

Description

Display on alarm

Select True to to automatically open and display the attachment when the alarm is going from Normal to Alarm state.

Show milliseconds

Select True to display the alarm timestamp in milliseconds.

  • General Information Properties – Basic Tab
  • Alarms Overview