earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funcionalidades: Alarmas
Versión del producto: 2.0, 2.1, 3.0, 3.1
13/12/2018

Alarms Pane and Alarm View Icons

Use the alarm state icons in the Alarms pane and Alarm View to get information about the state of the alarms.

Tabla: Alarms Pane and Alarm View Icons

Icon

Description

 
action_zoom_plus_stroke

Normal

Indicates that the alarm is idle and the variable the alarm monitors does not satisfy the configured alarm criteria. Para obtener más información, consulte Alarm States .

 
action_zoom_plus_stroke

Alarm

Indicates that an alarm is triggered. Para obtener más información, consulte Alarm States .

 
action_zoom_plus_stroke

Acknowledged

Indicates that a user has acknowledged the alarm. The problem that caused the alarm has not been corrected. Para obtener más información, consulte Alarm States .

 
action_zoom_plus_stroke

Reset

Indicates that the problem that caused the alarm is corrected. A user needs to acknowledge the alarm to change the alarm state to normal. Para obtener más información, consulte Alarm States .

 
action_zoom_plus_stroke

Disabled

Indicates that the alarm is disabled by a user. Disabled alarms are by default hidden in the Alarms pane and Alarm View. Para obtener más información, consulte Alarm States .

 
action_zoom_plus_stroke

Fault

Indicates that the value reported from hardware, such as a BACnet device, is not trustworthy. Para obtener más información, consulte Alarm States .

 
action_zoom_plus_stroke

Attachment

Indicates that the alarm has an object attached. Para obtener más información, consulte Archivos adjuntos de alarma .

  • Alarm States
  • Cambio de la ordenación de los estados de alarma
  • Archivos adjuntos de alarma
  • Panel Alarmas y vista Alarma
  • The Alarm Is Disabled and Cannot Be Enabled