earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
功能: 警报
产品版本: 2023
2022/12/16

Alarms Pane and Alarm View Icons

Use the alarm state icons in the Alarms pane and Alarm View to get information about the state of the alarms.

表格: Alarms Pane and Alarm View Icons

Icon

Description

 
action_zoom_plus_stroke

Normal

Indicates that the alarm is idle and the variable the alarm monitors does not satisfy the configured alarm criteria. 有关更多信息,请参阅 Alarm States .

 
action_zoom_plus_stroke

Alarm

Indicates that an alarm is triggered. 有关更多信息,请参阅 Alarm States .

 
action_zoom_plus_stroke

Acknowledged

Indicates that a user has acknowledged the alarm. The problem that caused the alarm has not been corrected. 有关更多信息,请参阅 Alarm States .

 
action_zoom_plus_stroke

Reset

Indicates that the problem that caused the alarm is corrected. A user needs to acknowledge the alarm to change the alarm state to normal. 有关更多信息,请参阅 Alarm States .

 
action_zoom_plus_stroke

Disabled

Indicates that the alarm is disabled by a user. Disabled alarms are by default hidden in the Alarms pane and Alarm View. 有关更多信息,请参阅 Alarm States .

 
action_zoom_plus_stroke

Fault

Indicates that the value reported from hardware, such as a BACnet device, is not trustworthy. 有关更多信息,请参阅 Alarm States .

 
action_zoom_plus_stroke

Attachment

Indicates that the alarm has an object attached. 有关更多信息,请参阅 报警附件 .

  • Alarm States
  • 更改报警状态排序顺序
  • 报警附件
  • 报警窗格和报警视图
  • The Alarm Is Disabled and Cannot Be Enabled