earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos WebReports
Funcionalidades: Informes
Versión del producto: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
16/12/2021

Alarms Per Server Report

The Alarms Per Server report provides information about the number and type of alarms that have been triggered for a particular EcoStruxure BMS server. You can use the report to identify the most frequent alarms on a particular EcoStruxure BMS server and then benchmark the operations of your building system. For example, suppose there are numerous alarms in Building A, but more staff are present in Building B. The report could indicate that you need to increase the staff in Building A in order to meet the operational needs of the building.

The following table shows the input parameters for the report.

Tabla: Alarms Per Server Input Parameters

Input Parameters

Description

Start report date/time

Specifies the start date and time of the triggered alarms.

End report date/time

Specifies the end date and time of the triggered alarms.

Date range filter

Specifies the date range of an operation, such as an alarm trigger, the running of a report schedule, or a read by the Reporting Agent.

For example, if you select Last 7 days for an alarm report, the report displays information about all alarms that were triggered during the last 7 days. If you select Last 7 days for the Report schedule report, the report displays information about all Report schedules that were run during the last 7 days. If you select Last 7 days for the Reporting Agent report, the report displays information about all Reporting Agent reads that occurred during the last 7 days.

Select Fixed date if you entered a Start report date/time and an End report date/time .

Acknowledged only

Specifies whether you want to report on Acknowledged alarms only or to report on all alarm activity.

Server

Specifies the EcoStruxure BMS server that manages the alarms.

Report view

Specifies the format, such as a table, for displaying the report.

Show top

Specifies a number used to filter the top most frequently occurring alarms.

  • Factory Supplied Reports
  • Production Reports
  • WebReports Submit Form Page