earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Virtual Project Servers, WebStation
Functionalities: Schedules
Product version: 3.2, 3.3, 2022
7/20/2021

Analog Schedules

An analog schedule controls a device that gauges the output in real numbers. The real numbers include positive or negative numbers, fractions, and decimal values.

For example, you can create an analog schedule to regulate a thermostat setpoint in an office area. To control the temperature from 08:00 to 17:00, you can set the value to 22 °C (72 °F) when the schedule is active and 16 °C (62 °F) when the schedule is inactive.

 
action_zoom_plus_stroke Analog Schedule
Figure: Analog Schedule
  • Schedule Types
  • Creating an Analog Schedule
  • Modifying a Schedule Using the Text View
  • Modifying a Schedule Using the Graphic View