earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Produits : Enterprise Central, Enterprise Server, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
23/10/2018

Archive Folders, Files, and Names

As part of the archive process, the system creates uniquely named archive files and folders that identify the type of archive (manual or scheduled) and the date on which the archive was performed.

 
action_zoom_plus_stroke Archives folder on Enterprise Server
Figure : Archives folder on Enterprise Server

By default, these folders are located in the Archives directory where the Enterprise Server or Enterprise Central are installed. However, you can change the directory to another valid location.

Archive Folder Names

During the archive process, the system creates a new folder in the path specified in the Archive Settings Manager. The system generates and then places the CSV or XML files within this folder. To prevent accidental overwriting, the system uses the Method_date.file extension format, which makes the folder name unique. For example, if you manually generate an archive on April 11, 2012, the system creates a folder named Manual_Archive20120411 (yyyymmdd). If you generate an archive the following day, the system creates a new folder with the new date.

Archive System Resource Files

When archiving is enabled, the system creates resource files that collect the data from the selected extended trend logs prior to archiving. The system names the files using random hexadecimal characters, such as a2d9e877, and then places them in the path specified in the Archive Settings Manager. These files should not be deleted.

File Names for Extended Trend Log Archives

The system names extended trend log archive files using the Method_(Address)_date.file extension format. If you generate a manual archive in CSV format for extended trend logs on on July 8, 2012, the system names the file, Manual_Archive_(Server_1_<Extended_Trend_Log name>)_2012-07-01_2012-07-08.csv.

File Names for Events Log Archives

The system names the event log archives using the Method_(EventLog)_date.file extension format. If you manually generate an archive on April 11, 2012 for the Alarm, User, and System events, the system names the archive file Manual_Archive_(Server_1_System_Events_EventLog_EventRecords)_2012-04-02_2012-04-11.csv.

Unique Archive File Names

If you generate more than one archive file on the same date, the system appends a number to the end of each similarly named archive to ensure that the files are not overwritten. For example, if you manually generate an archive named Manual_(Server_1_System_Events_EventLog_EventRecords)_2012-04-02_2012-04-11.csv and immediately generate another identical archive, the system names the second archive, Manual_(Server_1_System_Events_EventLog_EventRecords)_2012-04-02_2012-04-11_1.csv. Using the appended number (_1), the system creates a unique name for the second archive with the same method on the same date.

Archive Log Contents

You use a structured database editor to view archive information in rows and columns, which may contain text strings, paths, identities, or enumeration values.

Pour plus d'informations, voir Archive Log Contents .

  • Archiving Overview
  • Archive Log Contents