You generate an archive by selecting either a CSV or XML format. You can store the archive in Enterprise Server, Enterprise Central, or define a different location.
Method |
Description |
CSV |
Comma Separated Values is a standard text file that stores spreadsheet or database information in a simple table format. Each record is on a separate line and each field within that record is separated by a delimiter, such as a comma. |
XML |
Extensible Markup Language is a markup language that defines a set of rules for formatting documents. Primarily, XML is used to structure, transport, and store data rather than to display data. |
You define a path to store the archives on your file system.
The preferred path is to the Archives folder in the Enterprise Server or Enterprise Central:
Enterprise Server: ..\ProgramData\Schneider Electric EcoStruxure\Building Operation <version>\Enterprise Server\db
Enterprise Central: ..\ProgramData\Schneider Electric EcoStruxure\Building Operation <version>\Enterprise Central\db
You can use another location, such as a network drive or external memory device. To ensure that the new location is valid, you can prompt the system to validate the path. Więcej informacji zawiera Enabling the Archiving Function and Defining the Archive Folder .