earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 2024, 7.0
10/30/2025

Archiving Settings Properties – Basic Tab

Use the ​ Basic tab to enable the archiving function, set delay, and select the format of the archive file.

 
action_zoom_plus_stroke Archive Settings Basic properties tab
Figure: Archive Settings Basic properties tab

Table: Archive Settings Basic Tab

Component

Description

Enabled

Select True to activate the archiving function.

Path

Type the path to the location where you want to create your archive.

IsValidPath

Select True to indicate the objects have passed the validation.

Output format

Select the output format of the archive. For more information, see Archive Formats and Storage .

  • Archiving Overview
  • Manual and Scheduled Archiving
  • Archive Formats and Storage
  • Archiving Settings Properties – Content Tab
  • Enabling the Archiving Function and Defining the Archive Folder
  • Creating a Scheduled Archive
  • General Information Properties – Basic Tab
  • References Tab