earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos Enterprise Central, Enterprise Server, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
23/10/2018

Archiving Settings Properties – Basic Tab

Use the ​ Basic tab to enable the archiving function, set delay, and select the format of the archive file.

 
action_zoom_plus_stroke Archive Settings Basic properties tab
Figura: Archive Settings Basic properties tab

Tabla: Archive Settings Basic Tab

Component

Description

Enabled

Select True to activate the archiving function.

Path

Type the path to the location where you want to create your archive.

IsValidPath

Select True to indicate the objects have passed the validation.

Output format

Select the output format of the archive. Para obtener más información, consulte Archive Formats and Storage .

  • Archiving Overview
  • Manual and Scheduled Archiving
  • Archive Formats and Storage
  • Archiving Settings Properties – Content Tab
  • Enabling the Archiving Function and Defining the Archive Folder
  • Creating a Scheduled Archive
  • General Information Properties – Basic Tab
  • References Tab