earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: Enterprise Central, Enterprise Server, Project Configuration Tool
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018/10/23

Archiving Settings Properties – Basic Tab

Use the ​ Basic tab to enable the archiving function, set delay, and select the format of the archive file.

 
action_zoom_plus_stroke Archive Settings Basic properties tab
图: Archive Settings Basic properties tab

表格: Archive Settings Basic Tab

Component

Description

Enabled

Select True to activate the archiving function.

Path

Type the path to the location where you want to create your archive.

IsValidPath

Select True to indicate the objects have passed the validation.

Output format

Select the output format of the archive. 有关更多信息,请参阅 Archive Formats and Storage .

  • Archiving Overview
  • Manual and Scheduled Archiving
  • Archive Formats and Storage
  • Archiving Settings Properties – Content Tab
  • Enabling the Archiving Function and Defining the Archive Folder
  • Creating a Scheduled Archive
  • General Information Properties – Basic Tab
  • References Tab