earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
10/23/2018

Archiving Settings Properties – Content Tab

Use the Content tab to add events and trend logs to the archive.

 
action_zoom_plus_stroke Archive Settings Content tab
Figure: Archive Settings Content tab

Table: Archive Settings Basic Properties Tab

Component

Description

Alarm

Select True to include Alarm events in the archive.

User

Select True to include User events in the archive.

System

Select True to include System events in the archive.

Logs

Displays the logs you have selected to be archived.

 
action_zoom_plus_stroke

Click to add a new trend log to the archive.

 
action_zoom_plus_stroke

Click to change the trend log to be archived.

 
action_zoom_plus_stroke

Click to remove a trend log from the archive.

  • Archiving Overview
  • Archive Folders, Files, and Names
  • Archiving Settings Properties – Basic Tab
  • Removing Extended Trend Logs from the Archive
  • General Information Properties – Basic Tab
  • References Tab