Produkty: Enterprise Central, Enterprise Server, Project Configuration Tool
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-10-23

Archiving Settings Properties – Content Tab

Use the Content tab to add events and trend logs to the archive.

 
action_zoom_plus_stroke Archive Settings Content tab
Rysunek: Archive Settings Content tab

Tabela: Archive Settings Basic Properties Tab

Component

Description

Alarm

Select True to include Alarm events in the archive.

User

Select True to include User events in the archive.

System

Select True to include System events in the archive.

Logs

Displays the logs you have selected to be archived.

 
action_zoom_plus_stroke

Click to add a new trend log to the archive.

 
action_zoom_plus_stroke

Click to change the trend log to be archived.

 
action_zoom_plus_stroke

Click to remove a trend log from the archive.

  • Archiving Overview
  • Archive Folders, Files, and Names
  • Archiving Settings Properties – Basic Tab
  • Removing Extended Trend Logs from the Archive
  • General Information Properties – Basic Tab
  • References Tab