earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebReports
Functionalities: Reports
Product version: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
12/16/2021

Assign Default Reports Page

Use the Assign Default Reports page to assign a template to a type of object. The template is then used when you generate a default report in WorkStation. For more information, see WebReports Main Page .

 
action_zoom_plus_stroke Assign Default Reports page
Figure: Assign Default Reports page

Table: Assign Default Reports Page

Component

Description

Type of Object

Lists the type of objects associated with the templates.

Default Report Templates

Select to assign a template to a type of object. The template is used when you generate a default report.

  • Default Reports
  • WebReports Main Page