earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: WebReports
功能: 报告
产品版本: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
2021/12/16

Assign Default Reports Page

Use the Assign Default Reports page to assign a template to a type of object. The template is then used when you generate a default report in WorkStation. 有关更多信息,请参阅 WebReports Main Page .

 
action_zoom_plus_stroke Assign Default Reports page
图: Assign Default Reports page

表格: Assign Default Reports Page

Component

Description

Type of Object

Lists the type of objects associated with the templates.

Default Report Templates

Select to assign a template to a type of object. The template is used when you generate a default report.

  • 默认报告
  • WebReports Main Page